AXIS#.IL.COGCOMP.TEACH.V

Description

The constant velocity used during the Cogging Compensation teach.

Versions

Action Version Notes
Implemented 02-08-00-000

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value 1 rpm

Data Type

Float
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
AXIS1.IL.COGCOMP.TEACH.V

500ah

21h

Unsigned32

Velocity

-

Read/Write

No

AXIS2.IL.COGTABLE.TEACH.V

510ah

21h

Unsigned32

Velocity

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.COGCOMP.TEACH.V

5852

16DC

Signed32

Read/Write

Velocity

AXIS2.IL.COGCOMP.TEACH.V

71388

116D

Signed32

Read/Write

Velocity

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.COGCOMP.TEACH.V

5852

Float

Read/Write

Velocity